Is there any ready to use UI solutions(lcd screen,keypad or touchpad) with kinetis freedom KW41Z development board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any ready to use UI solutions(lcd screen,keypad or touchpad) with kinetis freedom KW41Z development board?

863 Views
satsok_n
Contributor III

I am using freedom KW41Z development board and for the needs of the project which I work for I have to create a User Interface. I would like to know if there are any ready to use parts like lcd screen, touchpad or keypad. I want to plug them in KW41Z, not control them with other boards since in my project power consumption is quite important.(I can only use KW41Z). 

0 Kudos
Reply
1 Reply

780 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Sorry but we do not have a ready to use code for what you are looking for, still, you can either use the available examples in the SDK for what you need such as the gpio_interrupt and adapt it to your needs.

Another thing that you can try to do is to look for an example in the community for another M0+ kinetis device and try to adapt it to your needs.

Regards ,

Estephania

0 Kudos
Reply