Is there any otg example of FRDM-KL26Z?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any otg example of FRDM-KL26Z?

1,327件の閲覧回数
alfchen
Contributor I

Hello,

I am using frdm-kl26z, i have downloaded SDK_2.0_FRDM-KL26Z, but there are not otg-related example in it.

The only document on kl26 otg is KL26P121M48SF4RM.pdf, which have few pages discribe usb otg registers.

It would be greet if there are some exmaple code or detailed document , is there any otg example of frdm-kl26z?

I have downloaded Freescale USB Stack v4.0.3 , but it seems that the Freescale USB Stack do not support frdm-kl26z by default.

Thanks,

Alf

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,096件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Alf,

We have provided the api function for otg of usb in only SDK2.1 version, but currently, there is only SDK2.0 version package for Kl26.

I have downloaded the SDK2.1 for FRDM-K64F, there is otg directory in the SDK package, if you are urgent, you can refer to it. But we have not example for otg.

You can download SDK from the link:

http://www.nxp.com/ksdk

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 件の賞賛
返信

1,096件の閲覧回数
alfchen
Contributor I

Hi xiangjun.rong,

Thank you for your reply. I get SDK download url from MCUXpresso SDK Builder, there are no option to select SDK version in SDK Builder, and SDK version is V2.0 by default. As a result , i can only download SDK V2.0 .

BR,

Alf

0 件の賞賛
返信

1,096件の閲覧回数
mjbcswitzerland
Specialist V

Hi Alf

See http://www.utasker.com/kinetis/FRDM-KL26Z.html
and
http://www.utasker.com/kinetis/TEENSY_LC.html

Includes KL26 USB stack for Audio, CDC, RNDIS, MSD, HID [or composites of these]
(Including KL26 and USB simulation for learning or accelerated developments).
Industrial quality code proven in many Kinetis based products since 2011 (and Coldfires since 2008).

Regards

Mark

http://www.utasker.com/kinetis.html

0 件の賞賛
返信