Hi all,
Is there any library can be used on K60 board? If no, can libmodbus library be use on it?
Thanks.
解決済! 解決策の投稿を見る。
Hi
There is a (commercial) MODBUS extension package to the uTasker project for Kinetis which runs 'out-of-the-box' on a K60 tower board:
http://www.utasker.com/modbus.html
It does master and/or slave ASCII/RTU and Modbus TCP and can be used as Modbus gateway or router. Multiple masters and slaves can be used on multiple UARTS and/or TCP sockets as well as via USB.
Detailed user's guide: http://www.utasker.com/docs/MODBUS/uTasker_MODBUS.PDF
Regards
Mark
Hi
There is a (commercial) MODBUS extension package to the uTasker project for Kinetis which runs 'out-of-the-box' on a K60 tower board:
http://www.utasker.com/modbus.html
It does master and/or slave ASCII/RTU and Modbus TCP and can be used as Modbus gateway or router. Multiple masters and slaves can be used on multiple UARTS and/or TCP sockets as well as via USB.
Detailed user's guide: http://www.utasker.com/docs/MODBUS/uTasker_MODBUS.PDF
Regards
Mark
Hi Mark,
And any other free one?
I am working with K64 and KDS with MQX
Could i use libmodbus?
Thanks and best regards
If you find one, please post the information here!
Hi
It is worth going to www.usb.org since they list various Modbus SW resources: modbus.org/tech.php
Or searching "opensource MODBUS" or "free MODBUS" gives a list that can be investigated
Regards
Mark