Is there any library for modbus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any library for modbus?

Jump to solution
5,728 Views
danielchai
Senior Contributor I

Hi all,

Is there any library can be used on K60 board? If no, can libmodbus library be use on it?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
3,397 Views
mjbcswitzerland
Specialist V

Hi

There is a (commercial) MODBUS extension package to the uTasker project for Kinetis which runs 'out-of-the-box' on a K60 tower board:

http://www.utasker.com/modbus.html

It does master and/or slave ASCII/RTU and Modbus TCP and can be used as Modbus gateway or router. Multiple masters and slaves can be used on multiple UARTS and/or TCP sockets as well as via USB.

Detailed user's guide: http://www.utasker.com/docs/MODBUS/uTasker_MODBUS.PDF

Regards

Mark

View solution in original post

0 Kudos
Reply
4 Replies
3,398 Views
mjbcswitzerland
Specialist V

Hi

There is a (commercial) MODBUS extension package to the uTasker project for Kinetis which runs 'out-of-the-box' on a K60 tower board:

http://www.utasker.com/modbus.html

It does master and/or slave ASCII/RTU and Modbus TCP and can be used as Modbus gateway or router. Multiple masters and slaves can be used on multiple UARTS and/or TCP sockets as well as via USB.

Detailed user's guide: http://www.utasker.com/docs/MODBUS/uTasker_MODBUS.PDF

Regards

Mark

0 Kudos
Reply
3,397 Views
albertolubeiro
Contributor III

Hi Mark,

And any other free one?

I am working with K64 and KDS with MQX

Could i use libmodbus?

Thanks and best regards

0 Kudos
Reply
3,397 Views
dave408
Senior Contributor II

If you find one, please post the information here!

0 Kudos
Reply
3,397 Views
mjbcswitzerland
Specialist V

Hi

It is worth going to www.usb.org since they list various Modbus SW resources: modbus.org/tech.php

Or searching "opensource MODBUS" or "free MODBUS" gives a list that can be investigated

Regards

Mark

0 Kudos
Reply