Hi Alfredo Perez Grovas,
In my opinion, the main problem is not in the NXP kinetis chip side, it should in the SD card side.
Just take kingmax SD card as an example,

Even you check the SD specification, you can find this information:

The initialization volage is 2V to 3.6V, that's the root reason why you can't find it. This is the SD card feature, and as I know, this is the standard feature.
The K28 can work with 1.8V, but the SD card can't work.

So, if you want to use the SD card, you need to use the voltage at about 3V.
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------