Is there a Mil-Spec version of the KL43P64M48SF6 processor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a Mil-Spec version of the KL43P64M48SF6 processor?

1,319 Views
spflanze
Contributor I

I am looking for ultra low power in Mil-Spec. I need 80uA/MHz or less.

Labels (1)
0 Kudos
Reply
2 Replies

459 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Stephen Pflanze,

Regarding to the low-power consumption level, the KL43 can down to 54uA/MHz in very low power run mode.

And you can learn the more information from the attachment.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

459 Views
spflanze
Contributor I

I still need to know if this processor is available in a Mil-Spec version. I did not see any information about Mil-Spec in the PDF attached to the message on your website.

0 Kudos
Reply