Is the UART0 of the Kinetis K60 combatible with PL011 interrupt-driven libraries?

cancel
Showing results for 
Search instead for 
Did you mean: 

Is the UART0 of the Kinetis K60 combatible with PL011 interrupt-driven libraries?

269 Views
benjaminmorris
Contributor I

I am developing code for the K60, and I would like to avoid using MQX. Is the UART0 compatible with any PL011 interrupt-driven libraries?

If it is compatible, which library is best?

If not, where can I find interrupt-driven libraries for the K60 UART0 and/or documentation on the differences?

Also, will these libraries run under QEMU in interrupt-driven mode?

Labels (1)
0 Kudos
0 Replies