Is the Exposed Die Attach Pad on the MK02FN128VFM10 a ground pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the Exposed Die Attach Pad on the MK02FN128VFM10 a ground pin?

802 Views
mindchasers
Contributor III

Hello,

I don't see it called out in the datasheet whether the Exposed Die Attach Pad on the MK02FN128VFM10  (32-pin QFN package) is actually a ground.

Please confirm it's a ground and should be tied into a ground plane. 

If it's not a ground, is it OK to tie it to ground? 

If it's not OK to tie it to ground, then what is the recommendation on dealing with it on the PCB board?

Thank you,

Bob

0 Kudos
Reply
1 Reply

610 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Robert Cochran

Yes, in kinetis devices it is connected to ground. I recommend you checking the AN1902:

https://www.nxp.com/docs/en/application-note/AN1902.pdf 

In "4.2.2 Guideline for exposed pad land patterns" you can find a more specific explanation.

Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply