Is source of CMSIS-DAP available?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is source of CMSIS-DAP available?

ソリューションへジャンプ
6,239件の閲覧回数
kai_liu
Senior Contributor I

Recently I found some incomplete source release of CMSIS-DAP for NXP/ST ARM. I want to know if it is available from FSL for its MCU, like FRDM-KL25Z or other low-cost platforms?

If yes, then we can build a custom CMSIS-DAP debugger without disable on-board connection between K20 and KL25Z.

Allan

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
3,100件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Liu Kai,

FRDM-KL25Z board provides P&E OpenSDA debugger tool, which could use to debug other Kinetis chip.

About how to use FRDM-KL05Z board debug other Kinetis chip, You could find related info from below link:

https://community.freescale.com/thread/306394

And Freescale also provide Kinetis tower board, which with P&E OSJTAG debugger tool on board.

Wish it helps.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,100件の閲覧回数
drewbarbier
Contributor I

You can download CMSIS-DAP deliverables from ARM via the link below (requires login).

https://silver.arm.com/browse/CMSISDAP

Drew

0 件の賞賛
返信
3,100件の閲覧回数
kai_liu
Senior Contributor I

Thank you, all of you.

I have registered and downloaded the deliverable. I finally realize one issue: all of the sources at my hand, including NXP version, STM version, FSL version are all built with Keil ARM uVision 4.6+. And my evaluation copy can not support it. It will stop at linking and tell me "RL-ARM can not be supported in your license"!

Since I can not offer a complete license from Keil, too expensive. I have to port it to IAR/GNU toolchain. Otherwise I have to copy the hardware design with prebuilt binary releases, like LPC11U37 and FSL K20 OpenSDA.

And I have to design another bootloader for K20 if I use its binary release. I have checked its S19, the application starts from 0x8000. It means the leading 32KB is taken by MSD bootloader.

My optimize solution for an open source CMSIS-DAP should be:

  • KL25Z128 (smaller package) with buffer output to JTAG/SWD
  • MSD bootloader (not available yet from FSL)
  • CMSIS-DAP build with GNU/IAR
  • OpenOCD gdbserver or PyOCD
  • Any IDE, including Keil/IAR/Eclipse with GNU or CMSIS-DAP RDDI.
0 件の賞賛
返信
3,100件の閲覧回数
JAlvarez
Contributor II

A Keil MDK Pro license is not required for building the ARM DAP examples if you use the USB device stack source code. This stack was open sourced by the mbed/CMSIS-DAP project.

https://github.com/mbedmicro/CMSIS-DAP/tree/master/shared/USBStack

These projects at Github include Keil project files to use Freescale K20 MCUs as CMSIS-DAP debuggers and may be useful for your purposes. The mbed/CMSIS-DAP project also implements flash programming of targets via USB MSD, a USB CDC serial port, a USB bootloader and the Keil RTX RTOS.

mbedmicro/CMSIS-DAP · GitHub

micromint/mbed-DAP · GitHub

The mbed library also supports GCC and IAR. It shouldn't be difficult to adapt the GCC and IAR toolchain files from the mbed library to the mbed CMSIS-DAP project.

mbedmicro/mbed · GitHub

0 件の賞賛
返信
3,100件の閲覧回数
kai_liu
Senior Contributor I

Thanks, I got it running on FRDM-K20.

0 件の賞賛
返信
3,101件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Liu Kai,

FRDM-KL25Z board provides P&E OpenSDA debugger tool, which could use to debug other Kinetis chip.

About how to use FRDM-KL05Z board debug other Kinetis chip, You could find related info from below link:

https://community.freescale.com/thread/306394

And Freescale also provide Kinetis tower board, which with P&E OSJTAG debugger tool on board.

Wish it helps.

0 件の賞賛
返信