I am trying to get the TWR-K600D100M to function with the old TWR-LCD controller. I was going to purchase the TWR-K60N512 but noted on the page that this was not recommended now so purchased the recommended alternative. This appears not to offer any support for this display. Also I notice on the forums that people are using eGUI 3.0 but I can only find version 2.1. Any idea where I can get the newer version from?
Hi Ian,
I checked with our developer of eGUI and the 3.0 release should happen near end of January 2014.
Regards,
David
eGUI on the Freescale.com/egui web site still reports to be version 2.1 dated 4/14/2011.
Is there an update to this yet?
Thanks
Ian
Hi Lan,
Any progress on this issue?
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
You can grab it from here now: Freescale eGUI: Graphical LCD Driver for MCUs|Freescale
It has projects specifically for K60D100M
-Anthony