Is it possible to start the kinetis into a flash swapped block?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to start the kinetis into a flash swapped block?

1,178 Views
ngarto
Contributor I

Is it possible to, on hard reset, start the kinetis directly into, for example, bank 1, swapped to map to address 0? Or does it always start in bank0 and require the flash swap commands to be executed? I'm wondering if there's a mechanism to persist the swap state.

Labels (1)
Tags (3)
0 Kudos
1 Reply

420 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

When the Kinetis product finish the SWAP procedure, the swapped flash block will as Flash start up block whatever the hard or soft reset.

It will continue to as start up flash block until next swap operation happens.

More detailed info about Kinetis  SWAP feature, please check AN4533.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos