Is it possible to connect VREFH to 0V on the Kinetis KE15Z family?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to connect VREFH to 0V on the Kinetis KE15Z family?

跳至解决方案
3,440 次查看
MarcoAEE
Contributor II

Hi,

i'm using a MKE15Z128VLL7 with available VREFH pin. VREFH will be connected to a 4.096V shunt precision reference (LM4040).
I have to create a project that allows the system to be brought to an ultra low power condition. For this reason, when I put the MCU to deep sleep I would like to turn off all peripherals including the shunt precision reference. Essentially there will be a battery supplying the 5V to the MCU VDD pin and shutting down the 5V that goes elsewhere.
From datasheet it shows that the minimum voltage of VREFH is 2.5V, I wonder if for some reason I can damage the MCU if I bring it to 0V.

Datasheet:

MarcoAEE_0-1683820664240.png

Thank you

Marco

 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,430 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @MarcoAEE 

It is not recommended to use values different to the operating conditions.

Best Regards, Miguel.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,423 次查看
bobpaddock
Senior Contributor IV
Removing power from the module effectively puts an unknown impedance on the internal bus. Current levels can go up.

A couple of diodes to drop the voltage lower than 4.096 might work to have the pin having some voltage when the system is powered down. Check that the difference between Vdd and VRefH doesn't get violated.
0 项奖励
回复
3,390 次查看
MarcoAEE
Contributor II

It's an interesting solution. But using shunt reference voltage like LM4040 it have relatively high quiescent current even if the voltage is lower than the reference voltage

I'm considering using a nano power reference voltage like REF35 that has a quiescent current below 1uA

Thank you

Marco

0 项奖励
回复
3,381 次查看
bobpaddock
Senior Contributor IV

I was assuming the 4040 was still having its power removed when in shutdown state.
Obviously needs isolated from the diode idea too.

0 项奖励
回复
3,356 次查看
MarcoAEE
Contributor II

Adding the diode in series to the reference voltage makes it meaningless. This is because the quality of the reference is subject to the fall of the diode and therefore not very precise and accurate

Thank you

0 项奖励
回复
3,343 次查看
bobpaddock
Senior Contributor IV
Obviously. Sadly text is a poor substitution for a schematic.
0 项奖励
回复
3,431 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @MarcoAEE 

It is not recommended to use values different to the operating conditions.

Best Regards, Miguel.

0 项奖励
回复