Is it possible to clock USB module with IRC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to clock USB module with IRC?

跳至解决方案
1,829 次查看
allankliu
Contributor III

Recently I am considering to design a macro USB dongle for Android (as HID/CDC device). Due to its limited space, I am trying to find a USB micro which can operate without external crystal. I know Microchip/Cypress can do, but STM claims that USB has to work with external crystal.

Can I use IRC(4MHz) of KL24/25Z as clock source for USB OTG?

Allan

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
1,614 次查看
pavel_krenek
NXP Employee
NXP Employee

It is impossible to use IRC for USB module because the internal reference clock does not have required accuracy which is strictly needed for peripheral USB.

Regard

Pavel

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,614 次查看
egoodii
Senior Contributor III

For just CDC, the CP2105 is a tiny self-contained UBS-to-serial device.  Smaller & cheaper than an osc.

0 项奖励
回复
1,615 次查看
pavel_krenek
NXP Employee
NXP Employee

It is impossible to use IRC for USB module because the internal reference clock does not have required accuracy which is strictly needed for peripheral USB.

Regard

Pavel

0 项奖励
回复
1,614 次查看
DerekLau
Contributor IV

It's not recommended to use internal clock for USB applications.