The datasheet says max LPTmr frequency is 24 Mhz. The reference guide says LPTmr can be driven from the "internal reference clock". The MCG_Lite can be configured for a 48 Mhz high frequency internal reference clock. But I don't see how to set the mcglite parameters to produce more than an 8 Mhz clock for the LPTmr. Currently I have:
const mcglite_config_t mcgliteConfig = {
.outSrc = kMCGLITE_ClkSrcHirc,
.irclkEnableMode = kMCGLITE_IrclkEnable,
.ircs = kMCGLITE_Lirc8M,
.fcrdiv = kMCGLITE_LircDivBy1,
.lircDiv2 = kMCGLITE_LircDivBy1,
.hircEnableInNotHircMode = true,
};
When I call CLOCK_GetFreq(kCLOCK_McgInternalRefClk), I get 8 Mhz, which the LPTmr does seem to be clocking at.
Thanks,
Chuck
解決済! 解決策の投稿を見る。
Hi Chuck,
it is not possible to clock the LPTMR higher frequency than 8 MHz if you are using internal oscillator. Clock module MCG Lite does not include FLL part and 8 MHz is maximum possible for this peripheral. But as you mentioned LPTMR can run on 24 MHz but with using external reference (OSCERCLK).
Best regards,
Pavel
Thanks Pavel!
Hi Chuck,
it is not possible to clock the LPTMR higher frequency than 8 MHz if you are using internal oscillator. Clock module MCG Lite does not include FLL part and 8 MHz is maximum possible for this peripheral. But as you mentioned LPTMR can run on 24 MHz but with using external reference (OSCERCLK).
Best regards,
Pavel