Is brownout detection available in MKL17Z64VFM4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is brownout detection available in MKL17Z64VFM4

1,747 Views
jagadeeshkumar
Contributor II

Hi

 I was looking at the data sheets there they mentioned no brown out is it is available or not.Could any one suggest me please.

Tags (1)
0 Kudos
Reply
4 Replies

1,607 Views
jagadeeshkumar
Contributor II

Yes,Is it possible to configure the LVD with user defined value.I want to detect power failure  when chip voltage is less than 2.8V is it possible.

0 Kudos
Reply

1,607 Views
bobpaddock
Senior Contributor III

Bits in the Reset Control Module will say if the reset is due to a power up:

/*lint -save -e514 */
rst_b |= (0U != (RCM_SSRS0 & (RCM_SSRS0_SPOR_MASK|RCM_SSRS0_SLVD_MASK))); /* Return not zero when Power On Reset or Low Voltage Detect bits are set */
/*lint -restore */

1,607 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jagadeesh Kumar

You can not configure LVD with user defined value, but you can select the voltage detect:

pastedImage_1.png

where:

pastedImage_2.png

Alternately you can use the "low voltage warning function" in the same module. I recommend you to check the chapter 15 of the Reference manual.

Hope this information helps you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,607 Views
bobpaddock
Senior Contributor III

Is "Low Voltage Detect" in the Power Management Controller what you are looking for?

0 Kudos
Reply