Is PTC5 of MKE1xZ pullup after POR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is PTC5 of MKE1xZ pullup after POR?

1,136 Views
isaotakashima
Contributor IV

According to table in 33.2.2 Pin properties, PTC5 is pullup after POR.

But no description for PTC5 in Table 34-1. Ports summary.

Which description is correct?

I believe that Table 34-1. Ports summary is correct.

Anyway I would like NXP to correct this typographical error as soon as possible.

In addition please let us know when NXP correct this.

Best regards,

Takashima

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

965 Views
jonson_chen
NXP Employee
NXP Employee

Hi Robin, 

Thanks a lot for your checking!

Hi Takashima,

The PTC5 is not pullup after POR, because it's default pin function is not debug function.

0 Kudos
Reply

965 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Takashima,

Test gpio_led_output example in SDK_2.3.0_FRDM-KE15Z, the PTC5 is not pullup after POR.

So I also believe that Table 34-1. Ports summary is correct.

PORTC_PCR5.PNG

I've will contact with the AE team for confirming. And I will inform you as soon as I get any feedback.

Thanks for your reporting!

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply