Is Kinetis K66 series a drop in replacement for K64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is Kinetis K66 series a drop in replacement for K64

Jump to solution
579 Views
geovarghese
Contributor II

Hi,

We are using MK64FN1M0VMD12 in one of our design. We would like to upgrade to the K66 series. Not so much for the memory but for the speed as it is 50% faster and it also has crypto engine if in the future we need to secure the LAN communication.  If we are to do this ideally it would have to be drop in replacement for hardware and code or I end up with different models that are not compatible. Can any one please confirm whether MK66FN2M0VMD18 can be used as a direct replacement in our case.

Regards,

Geo

0 Kudos
1 Solution
435 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Geo,

Definitely, the MK66FN2M0VMD18 can replace the MK64FN1M0VMD12 directly.
Have a great day,
Ping
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
436 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Geo,

Definitely, the MK66FN2M0VMD18 can replace the MK64FN1M0VMD12 directly.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos