Integrating IEEE 802.1X EAP Supplicant in MQX 4.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrating IEEE 802.1X EAP Supplicant in MQX 4.2

606 Views
Prabhath
Contributor I

Hello all,

We are working on an embedded application using MQX 4.2 on a Kinetis K66 MCU, and we now need to integrate IEEE 802.1X (EAP) support for port-level LAN authentication.

To proceed, I have a few questions:

  1. Are there any existing examples, demo projects, or documentation for implementing 802.1X on MQX 4.2 (or similar Freescale/NXP stacks)?

  2. Is there any lightweight 802.1X supplicant library available that’s suitable for resource-constrained MQX systems (preferably C-based and portable)?

  3. Has anyone tried porting wpa_supplicant or other embedded EAP clients into an MQX environment?

Any pointers, experience shares, or example projects would be greatly appreciated.

Thanks in advance!

Labels (1)
0 Kudos
Reply
3 Replies

582 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @Prabhath ,

Thanks for your post.

Please refer to the Freescale Embedded Solutions Based on ARM Technology Guide - Brochure.

The Kinetis K series does not support IEEE 802.1X by NXP. Only the KW series supports it.

In addition, MQX 4.2 is no longer supported. You can consider using MQX™ v5 Software Solutions | NXP Semiconductors.

Celeste_Liu_0-1746774384036.png

 

Celeste_Liu_1-1746774424094.png

Sorry for the inconvenience. Thank you for your understanding.

BRs,

Celeste

0 Kudos
Reply

463 Views
Prabhath
Contributor I
Thank you for the reply.

I would like to clarify a few more points. Is it possible to modify the application firmware to integrate IEEE 802.1X support?
0 Kudos
Reply

458 Views
Celeste_Liu
NXP Employee
NXP Employee

According to the RM, it supports IEEE 802.1q.

Celeste_Liu_0-1747201220484.png

 

0 Kudos
Reply