If I do not desire to use the 32KHz clock on a K64FN1M0VLL12 device is it okay to tie EXTAL32 to circuit ground?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

If I do not desire to use the 32KHz clock on a K64FN1M0VLL12 device is it okay to tie EXTAL32 to circuit ground?

691 次查看
rpflaum
Contributor II

If I do not desire to use the 32KHz clock on a K64FN1M0VLL12 device is it  okay to tie EXTAL32 to circuit ground?

标签 (1)
0 项奖励
回复
1 回复

608 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Robert,

As you know that the Extal32 is an input pin, if you do not use any crystal or clock source, it is okay to connect the Extal32 to GND directly.

BR

XiangJun Rong