INTMUX in larger Kinetis KL parts: Video explanation and demonstration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

INTMUX in larger Kinetis KL parts: Video explanation and demonstration

837件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

Newer and larger KL parts have something called an Interrupt multiplexer (INTMUX) which is used to extend the Cortex-M0+ NVIC limit of 32 peripheral interrupt to accommodate a larger set of peripheral interrupts.

The following video explains the details, code required to use it and demonstrates the RTC Alarm interrupt (extended peripheral interrupt) on the KL82 (FRDM-KL82Z): https://youtu.be/zKa5BoOhBrg

The binary of the code used in the video is available at http://www.utasker.com/kinetis/FRDM-KL82Z.html#INTMUX
and also shows running a dual OS on the board (uTasker + FreeRTOS).

Regards

Mark

http://www.utasker.com/kinetis.html

ラベル(2)
タグ(3)
0 件の賞賛
返信
0 返答(返信)