I need some pointers to find startup information.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I need some pointers to find startup information.

3,188 次查看
marktaylor
Contributor I

I have picked the KE04Z8VWJ4.

I have only programmed microchip MCU's before.

Where do I start?

I need to know the IDE.

I need a programmer.

Where do I find the datasheet about the language (assembly). I've looked everywhere.

I am on a deadline to get a project done.  Please help.

标签 (1)
0 项奖励
回复
4 回复数

2,831 次查看
dstraight
Contributor II

The Cyclone MAX (programmer) is very expensive.   

0 项奖励
回复

2,831 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Also you can use the Universal multilink FX

0 项奖励
回复

2,831 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Please let us know if you still needs help

Regards

Vicente Gomez

0 项奖励
回复

2,830 次查看
PatriciaTeran
Contributor III

Hi, Mark

You can find all the information regarding the IDE and the programmer in the next link

KE04 |Kinetis KE04 48 MHz Robustness MCUs|Freescale

As you can see, you could use different IDE, such as CW, KDS, etc. For the programmer, the one compatible with the KE04Z is the CycloneMax for P&E, is also listed in the link above.

I've attached the Reference Manual, which describes all the features, architecture and programming model of the KE04Z.

Hope it helps!

Regards

Patricia

0 项奖励
回复