I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds. Can anyone suggest me the feasibility for the same in KL46 controller ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds. Can anyone suggest me the feasibility for the same in KL46 controller ?

986 次查看
yusupkhan
Contributor II

I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds.  Can anyone suggest me the feasibility for the same in KL46 controller ?

标签 (1)
0 项奖励
回复
1 回复

789 次查看
mjbcswitzerland
Specialist V

Hi

You can select the source of the LPTMR clock.

If you have an 8MHz oscillator connected and use this as source you will have 125ns timer resolution.

regards

Mark

0 项奖励
回复