I just purchased a FEDM-K64F. I plugged it into a windows 10 PC. I tried to install the

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I just purchased a FEDM-K64F. I plugged it into a windows 10 PC. I tried to install the

Jump to solution
1,349 Views
malcolmmcdowell
Contributor I

I purchased a FRDM-K64F. I plugged it into a Windows 10 PC. After plugging the K64 board into the PC, I tried to install the mbed serial driver (mbedWinSerial_16466.exe). This application does not install and I get an error "mbed x64. Could not install the driver". After installing the serial driver, I tried to get the board to come up in boot-loader mode. The board doesn't come up in Bootloader" mode either. When the board is plugged in Windows pops up a message that says "USB device is not recognized".

A couple of questions

1) Should the mbed or openSDA serial driver to be installed for the FRDM-K64F?

2) After further reading I see a warning not to install the K64 with openSDA2 into a windows 10 PC. IS this the case

Has the board become corrupt?

Any help would be appreciated.

Malcolm

0 Kudos
1 Solution
1,040 Views
malcolmmcdowell
Contributor I

Thanks to both of you for your .replies. It is now working!!

Malcolm

View solution in original post

0 Kudos
3 Replies
1,041 Views
malcolmmcdowell
Contributor I

Thanks to both of you for your .replies. It is now working!!

Malcolm

0 Kudos
1,040 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Malcolm,

To provide the fastest possible support I want to point you to a similar question which has been answered on our NXP community. Please refer to https://community.nxp.com/docs/DOC-330935 to view the details.
To help NXP improve the technical support via communities please rate the answer given in the referred thread.


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,040 Views
mjbcswitzerland
Specialist V

Malcolm

You need to get the latest P&E driver and/or the latest mdeb one (P&E will allow debugging) since the version that was pre-installed was probably one that is not compatible with Win 10.


To install you may need to find a Win 7 PC though (or disable the way that Win 10, or Win 8 works with external drives - there are some guides to doing it if you search the Internet).

Your board should be OK once you have been able to install a suitable driver version.

Regards

Mark

0 Kudos