I have used MK70FN1M0VMJ12 it is not coming out of reset mode after connecting to debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have used MK70FN1M0VMJ12 it is not coming out of reset mode after connecting to debugger

928件の閲覧回数
shivakumarlv
Contributor I

Hi all

I have used MK70FN1M0VMJ12 in our project out of three boards two are working fine. i am using universal multilink as a debugger and programmer. after flashing program it is continuously going to reset mode instead of main(). I have checked REST pin it is high.also find the attachment of JTAG debugger. please advicejtag.jpg

0 件の賞賛
返信
1 返信

789件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Shivakumar,

After reviewing your JTAG connections I noticed that the pin 9 (PTA4/EZP_CS_b) is connected to ground, this will cause the MCU to enter in EZport mode after reset, we recommend to left this pin with a pull-up resistor to make sure it is kept high during the reset phase.

Please let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信