I have a TWR-K20D50M. I can get the MQX example to run for a USB Host. I cannot get the USB Device examples to run or enstantiate with my PC..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have a TWR-K20D50M. I can get the MQX example to run for a USB Host. I cannot get the USB Device examples to run or enstantiate with my PC..

423件の閲覧回数
GenkiKai
Contributor I

This is an out-of-the-box situation where I am evaluation this Microcontroller for use in a USB Device.  The USB Host code works just fine (I'm hosting a mouse right now).  I cannot get any of the USB Device examples to run at all.  I have tried the examples from "Freescale USB Stack v4.0.3" with no success as well.  Anu ideas?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

347件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Alan,

Please check the hardware configuration whether suits for the relevant USB demos or not.

2016-06-23_11-08-28.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

347件の閲覧回数
mjbcswitzerland
Specialist V

Hi

You can get TWR-K20D50M USB device (including accurate simulation) support from http://www.utasker.com/kinetis/TWR-K20D50M.html (even if only to check that your board works correctly).

Regards

Mark

0 件の賞賛
返信