I have a FRDM-KL25Z. Can I use it to program other Kinetis parts? If so, how?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have a FRDM-KL25Z. Can I use it to program other Kinetis parts? If so, how?

1,412件の閲覧回数
worstell
Contributor II

I have two  FRDM-KL25Z boards. Can I use them  program other Kinetis parts? If so, how?

I have some Kinetis parts and need to load programs to the Flash. There is no ROM bootloader on the parts I want to use. Can the FRDM-KL25Z or other low cost evaluation boards be used as a programmer for other Kinetis parts (separate parts, not on the development board but connected to it via SWD, serial, or whatever)?

Other vendors - TI, NXP, STM make this very easy, and I have used them all, but there are some Freescale parts that are better for my purposes.

On a related matter, the Flash code on one of my FRDM-KL25Z is messed up because I put some code in it that corrupted it. How can the original code be restored? A Freescale applications engineer worked with me for a while and was unable to do it.

g.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,272件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

yes, you can use the FRDM boards to program other boards.

You can use it as a programmer (with the MSD bootloader):

Using the Freedom Board as SWD Programmer | MCU on Eclipse

Or you can use it with the debugger (but not with the P&E firmware):

Using the FRDM-KL25Z with CMSIS-DAP to program non-Freescale ARM Microcontrollers | MCU on Eclipse

Debug External Processors with USBDM and Freedom Board | MCU on Eclipse

Segger J-Link Firmware for OpenSDAv2 | MCU on Eclipse

(carefully read for the last option the license agreement).

I hope this helps,

Erich

0 件の賞賛
返信

1,272件の閲覧回数
worstell
Contributor II

Erich Styger

replied to the discussion

"I have a FRDM-KL25Z. Can I use it to program other Kinetis parts? If so,

how?"

To view the discussion, visit:

https://community.freescale.com/message/546154?et=watches.email.thread#546154

>

0 件の賞賛
返信