I do not know what is wrong in the use of KE15Z FRDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I do not know what is wrong in the use of KE15Z FRDM

904 次查看
izhanghongcun
Contributor I

The program can't be downloaded or debuged  to the KE15Z FRDM.

Here is what I do to the KE15Z FRDM.

1 download the KSDK from kex.nxp.com.

2pastedImage_1.png

download the OpenSDA V2.1 J-link Firmware and put it into the bootloader.  

and then link the frdm with the PC via USB cable.

pastedImage_2.pngand the the com14 is communication com.

3 open the project by KDS(the latest version),build up the project

pastedImage_3.png

click on the debug button,

and then pastedImage_4.png

If you know where i am wrong ,please help me 

0 项奖励
回复
1 回复

797 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi aline,

Since you have download the OpenSDA V2.1 J-link Firmware, you should select GDB SEGGER J-Link debugger.

GDB SEGGER J-Link debugger.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复