I am woundering if I can use PTC4, PTC5, PTC6 and PTC7 as a GPIO and set them to logic high (Pull-Up) on PN# MK60DN512ZVLQ10 ? Thanks for your help.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am woundering if I can use PTC4, PTC5, PTC6 and PTC7 as a GPIO and set them to logic high (Pull-Up) on PN# MK60DN512ZVLQ10 ? Thanks for your help.

453 Views
karzanalbayati
Contributor I

I am new to work on this chip and I would like to get some help. Manufacturing part number is

MK60DN512ZVLQ10

0 Kudos
1 Reply

371 Views
pavel_krenek
NXP Employee
NXP Employee

Hi,

yes you can use these pins as GPIO. You can set the GPIO pin configuration for each of pins (OUTPUT, INPUT) with all appropriate feature as pull-up etc.