I am using the K64F with an attached JY-MCU (HC-05) as a master.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am using the K64F with an attached JY-MCU (HC-05) as a master.

839 Views
elinaiman
Contributor I

The slave is an android tablet. I am also using 2 IO lines on the K64F to connect to the EN and STATE lines on the HC-05.

When the slave shuts down, the master detects that via the STATE line on the HC-05. However when the slave starts up again, the HC-05 does not re-link to it automatically. I know that if you put the power OFF and then ON on the HC-05 it will re-connect.

On the K64F (J199) the power to the JY-MCU is connected directly to 3.3V line and not an IO line.

Do I have to use an IO line for the power.

Is there another procedure to get the JY-MCU to auto-connect without turning off the power. 

Thanks for your help.

Eli Naiman

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

753 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you provide the schematics of K64 and JY-MCU?

And what's the JY-MCU part number?


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply