How to use the LIN slave operation on the Kinetis KL17 LPUART module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the LIN slave operation on the Kinetis KL17 LPUART module

924 Views
ericliao
Contributor I

Hi

Whether there is a KL17 LPUART application note in a LIN slave operation or sample code for reference

pastedImage_1.png

Thanks

0 Kudos
Reply
1 Reply

755 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Eric Liao,

    We don't have the direct application note in a LIN Slave for KL17, but our AE team provided the UART validation code for your reference, which is for 120MHz part, but should be general , the LIN function nearly the same. Please kindly refer to attachment for more details.

    Besides this validation code, you also can refer to the KEA LIN stack, which can be download from this link:

LIN2.x and SAE J2602 Stack

   There also have the LIN Slave code for your reference.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply