How to update the firmware of MK20DX128VLF5 using USB(pendrive)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update the firmware of MK20DX128VLF5 using USB(pendrive)?

2,093件の閲覧回数
vigneshkumarp
Contributor III

Hi, We are using my own board of MK20DX128VLF5. Here we are copying the data(that was stored in flash) from controller to USB(pendrive) and it was done.

Now we need to update the firmware through USB(pendrive). Using code warrior10.6 the .S19 is generated and how can we use that .S19 file to reprogram the controller?  Or what is the procedure to update the firmware through USB(pendrive)?

0 件の賞賛
返信
3 返答(返信)

1,872件の閲覧回数
vigneshkumarp
Contributor III

And Sorry for the change in my questions. We changed the controller to MK22DX256VLF5 due to our requirement. And now we want to do the same for this controller to update the newer version of firmware through USB(pendrive).

Thanks.

0 件の賞賛
返信

1,872件の閲覧回数
mjbcswitzerland
Specialist V

Hi

USB-pendrive loaders are available for all Kinetis devices with USB at:
http://www.utasker.com/kinetis.html

Eg. of K22: http://www.utasker.com/kinetis/TWR-K22F120M.html

Documentation:
http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Regards

Mark

0 件の賞賛
返信

1,872件の閲覧回数
vigneshkumarp
Contributor III

Thanks Mark Butcher.

0 件の賞賛
返信