I was using PE MICRO universal multilink FX for debugging my project.
Ir was working fine for me until i updated my S32DS IDE and the firmware of PE MICRO universal multilink FX also got updated automatically when i tried to debug it.
Now PE MICRO universal multilink FX is not responding properly.
It is unable to enter DEBUG mode.

After clicking on ABORT, i got the following message.

I have re--installed the S32DS older version(the one without updates) still it is not working fine.
I think reverting back to older version of firmware may resolve the issue. If not, please suggest an alternative.
How to revert back to older version?
I have downloaded
http://www.pemicro.com/downloads/main_downloads_temp/201810031258175283381/multilink_universal_insta...
and installed firmware given here, but it didn't work...
Please revert back ASAP.
Regards,
Pritam