How to support micro SD card with file system on freeRTOS application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to support micro SD card with file system on freeRTOS application

1,433件の閲覧回数
zohargolan1
Contributor II

Hi,

I am using FreeRTOS integrated into Processor Expert and implementing it on K20 device.

How should I go about implementing a microSD interface with FAT file system.

Any comment will be highly appreciated

Zohar

0 件の賞賛
返信
3 返答(返信)

1,269件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Zohar,

you can use it either way: You can use only the SDK (there is a FatFS example in the SDK), or you can use the SDK with Processor Expert (but then it only suppports the fsl_* components), or you can use Processor Expert with the 'non-SDK' components. So you have freedom of choice :-)

Note that the FreeRTOS in the SDK is an older one (8.2.0) while the McuOnEclipse component is using the latest FreeRTOS (8.2.3).

I hope this helps,

Erich

0 件の賞賛
返信

1,269件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Zohar,

I'm using FreeRTOS with FatFS in several projects, see FatFs | MCU on Eclipse . There are sources/examples available on GitHub (see the links in the articles).

I hope this helps,

Erich

0 件の賞賛
返信

1,269件の閲覧回数
zohargolan1
Contributor II

Hi Erich,

As usual, thank you for the fast reply. The link you have send me is using the KSDK 1.2.0. I am using the freeROTS extention, which is not using the SDK. Is it going to be a problem or I can add the KSDK in processor expert?

Thank you,

Zohar

0 件の賞賛
返信