How to set and configure the KL03Z MCU to use the internal clock source to run the program?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to set and configure the KL03Z MCU to use the internal clock source to run the program?

跳至解决方案
1,737 次查看
waipongmok
Contributor I

Hi,

    How to set and configure the MKL03Z MCU to use the internal clock source to run the program in 48MHz/8MHz?

   

   Can you teach me?

   Thanks.

标签 (1)
0 项奖励
回复
1 解答
1,613 次查看
mjbcswitzerland
Specialist V

Hi

You can get some more real-word advice on the clocking at http://www.utasker.com/kinetis/MCG.html
For the KL03 you can clock directly from the IRC48M for 48MHz or from the LIRC for 2MHz or 8MHz.
If you were to use the uTasker project these are the settings to choose all options (with 48MHz valid):

    #define RUN_FROM_HIRC                                                // clock from internal 48MHz RC clock
  //#define RUN_FROM_LIRC                                                // clock from internal 8MHz/2MHz RC clock
    #if defined RUN_FROM_HIRC
        #define SYSTEM_CLOCK_DIVIDE  1                                   // 1..16
        #define BUS_CLOCK_DIVIDE     2                                   // 1..8 (valid for bus/flash and divisor is after the system clock divider)
    #elif defined RUN_FROM_LIRC
        #define RUN_FROM_LIRC_2M                                         // selet 2MHz rather than 8MHz
        #define SLOW_CLOCK_DIVIDE    1                                   // optionally divide the slow clock output (1, 2, 4, 8, 16, 32, 64 or 128)
        #define SYSTEM_CLOCK_DIVIDE  1                                   // 1..16
        #define BUS_CLOCK_DIVIDE     2                                   // 1..8 (valid for bus/flash and divisor is after the system clock divider)
    #else                                                                // run from the 32kHz osciallator
        #define SYSTEM_CLOCK_DIVIDE  1                                   // 32kHz
        #define BUS_CLOCK_DIVIDE     1                                   // 32kHz
    #endif

The actual code that configures the 48Mhz case is:

  //MCG_MC = MCG_MC_HIRCEN;                                              // this is optional and would allow the HIRC to run even when the processor is not working in HIRC mode
    MCG_C1 = MCG_C1_CLKS_HIRC;                                           // select HIRC clock source
    while ((MCG_S & MCG_S_CLKST_MASK) != MCG_S_CLKST_HICR) {             // wait until the source is selected
    }
    SIM_CLKDIV1 = (((SYSTEM_CLOCK_DIVIDE - 1) << 28) | ((BUS_CLOCK_DIVIDE - 1) << 16)); // prepare bus clock divides

Below is the uTasker KL03 simulator confirming the clock speeds obtained:

pastedImage_1.png

Regards

Mark

Kinetis for professionals: http://www.utasker.com/kinetis.html

在原帖中查看解决方案

2 回复数
1,613 次查看
sureshjaggal
Contributor III

Hi Wai Pong, 

If you are using processor expert then go to CPU component and choose Internal oscillator and disable the external oscillator. 

Regards,

Suresh Jaggal

0 项奖励
回复
1,614 次查看
mjbcswitzerland
Specialist V

Hi

You can get some more real-word advice on the clocking at http://www.utasker.com/kinetis/MCG.html
For the KL03 you can clock directly from the IRC48M for 48MHz or from the LIRC for 2MHz or 8MHz.
If you were to use the uTasker project these are the settings to choose all options (with 48MHz valid):

    #define RUN_FROM_HIRC                                                // clock from internal 48MHz RC clock
  //#define RUN_FROM_LIRC                                                // clock from internal 8MHz/2MHz RC clock
    #if defined RUN_FROM_HIRC
        #define SYSTEM_CLOCK_DIVIDE  1                                   // 1..16
        #define BUS_CLOCK_DIVIDE     2                                   // 1..8 (valid for bus/flash and divisor is after the system clock divider)
    #elif defined RUN_FROM_LIRC
        #define RUN_FROM_LIRC_2M                                         // selet 2MHz rather than 8MHz
        #define SLOW_CLOCK_DIVIDE    1                                   // optionally divide the slow clock output (1, 2, 4, 8, 16, 32, 64 or 128)
        #define SYSTEM_CLOCK_DIVIDE  1                                   // 1..16
        #define BUS_CLOCK_DIVIDE     2                                   // 1..8 (valid for bus/flash and divisor is after the system clock divider)
    #else                                                                // run from the 32kHz osciallator
        #define SYSTEM_CLOCK_DIVIDE  1                                   // 32kHz
        #define BUS_CLOCK_DIVIDE     1                                   // 32kHz
    #endif

The actual code that configures the 48Mhz case is:

  //MCG_MC = MCG_MC_HIRCEN;                                              // this is optional and would allow the HIRC to run even when the processor is not working in HIRC mode
    MCG_C1 = MCG_C1_CLKS_HIRC;                                           // select HIRC clock source
    while ((MCG_S & MCG_S_CLKST_MASK) != MCG_S_CLKST_HICR) {             // wait until the source is selected
    }
    SIM_CLKDIV1 = (((SYSTEM_CLOCK_DIVIDE - 1) << 28) | ((BUS_CLOCK_DIVIDE - 1) << 16)); // prepare bus clock divides

Below is the uTasker KL03 simulator confirming the clock speeds obtained:

pastedImage_1.png

Regards

Mark

Kinetis for professionals: http://www.utasker.com/kinetis.html