How to place my rbf file in the specified location of flash using the IAR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to place my rbf file in the specified location of flash using the IAR?

1,631 Views
zhailing
Contributor II

     Firsrtly,I get the rbf file through the Quartus II; want to config the fpga  using K64,how to place my rbf file in the specified address of flash using the IAR?

I place the rbf file to flash of K64 ; the expect address is ff000,

 pastedImage_1.png

 

pastedImage_2.png

The actual address is 0x410;  How should i do?

Thanks very much.

                                                                                                              zhai

0 Kudos
Reply
2 Replies

1,508 Views
zhailing
Contributor II

Now  i can place bin file in the specified address of flash;but another probelm is occur;pastedImage_1.png

there is no problem;

pastedImage_2.png

there is the problem

Error[Lp014]: cannot fit "Block ZI" (min size 0x3a9b0, alignment 0x4) into any of the ranges <[0x1fff0000-0x1fffffff], [0x20000000-0x2002fbff]> 

should I config the icf file ? how to config it?

thanks

0 Kudos
Reply

1,136 Views
alvamiler
Contributor I

Thank you for getting back to me so quickly.  

my location

0 Kudos
Reply