How to output system clock on a GPIO pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to output system clock on a GPIO pin

2,661件の閲覧回数
eigen
Contributor I

I have a Kinetis KL03Z board. I try to output the 48MHz system clock on a GPIO pin for some other use, but have a hard time finding related information of doing this. Please advise. Thanks.

タグ(1)
0 件の賞賛
返信
1 返信

2,341件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eigen,

You can use the CLKOUT pin to output the clock:

pastedImage_0.png

For example ,

- you can configure the bus clock to 48MHZ,

- then configure the PTA4 pin to CLKOUT through the register of  PORTx_PCRn -> MUX ;

- then configure the CLKOUT pin output BUS clock through

the register of "SIM_SOPT2" -> CLKOUTSEL to  " 010 "

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------