How to increase speed for SD card using SPI in FRDM-K20D50M board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to increase speed for SD card using SPI in FRDM-K20D50M board?

2,161件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hello

I am trying to store some counting values to check the speed of data storage in SD card so for 1 minute the counter is showing values upto 327. Which I think is less for my use, I need to increase the speed how can it be done? I am attaching the snapshot of speed setting for the SD card library.

pastedImage_0.png

and that of clock setting is

pastedImage_1.png

After all effort the maximum speed I could get is around 25 Mhz in place of 24 MHz. Kindly look into the matter.

Thanks & Regards

Amit Kumar

2 返答(返信)

1,093件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Amit:

I got confused with your statement:

After all effort the maximum speed I could get is around 25 Mhz in place of 24 MHz.

Do you mean you need more than 25 MHz? or that the maximum you are getting is 24 MHz?

If you look at the K20 50 MHz datasheet, you can see the maximum frequency for SPI module is 25 MHz:

SPI_freq.png

Hope this is somewhat useful.

Regards!

/Jorge Gonzalez

1,093件の閲覧回数
Amit_Kumar1
Senior Contributor II

HI Jorge

Thanks for your reply. I wanted to Tell that earlier I was having 24Mhz frequency but after changing clock setting I was able to increase the frequency upto 25 MHz. Actually I am running simple counter i++ and printing the value of i in a SD card in .txt format so for each minute the counter is giving value around 327. which I think is very less. I wanted around 100 counts per second but I am getting only 5.45 count per second. So how to increase the speed ?

Regards

Amit Kumar

0 件の賞賛
返信