How to get MK51DX128CLH7 into MCUXpresso?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to get MK51DX128CLH7 into MCUXpresso?

跳至解决方案
2,652 次查看
Bert2
Contributor II

Hi,

I'm trying to find out how to work with the MK51DX128CLH7 in Xpresso. I found the MK51DX256CLK10 in a SDK but not the 128.

Do I have to use the generic M4?

Thanks in advance,

regards,

Bert

0 项奖励
回复
1 解答
2,638 次查看
ErichStyger
Specialist I

Just an idea: KDS (Kinetis Design Studio) with Processor Expert supports that device:

ErichStyger_0-1647593299440.png

 

What I did for similar cases:

a) using the possibility to install Processor Expert in to MCUXpresso IDE (did that for earlier versions, have not checked if this is still possible with 11.5). see https://mcuoneclipse.com/2017/04/09/mcuxpresso-ide-installing-processor-expert-into-eclipse-neon/ how this would look like. Otherwise: I used KDS to generate everything and then used MCUXpresso (see b))

b) import/port the KDS project with Processor Expert. https://mcuoneclipse.com/2018/07/27/porting-processor-expert-projects-to-mcuxpresso-ide/

I know this is a bit challenging, but worked for me for several projects with devices which are not supported by the NXP MCUXpresso SDK.

I hope this helps,

Erich

 

在原帖中查看解决方案

4 回复数
2,648 次查看
ErichStyger
Specialist I

If they share the same peripherals, but are only different by the flash size, you should be able to use the smaller part, but change the linker file for the larger memory size.

0 项奖励
回复
2,643 次查看
Bert2
Contributor II

Hi, thanks for your quick answer. Unfortunately the devices differ in pinout (case) and peripherals.

0 项奖励
回复
2,639 次查看
ErichStyger
Specialist I

Just an idea: KDS (Kinetis Design Studio) with Processor Expert supports that device:

ErichStyger_0-1647593299440.png

 

What I did for similar cases:

a) using the possibility to install Processor Expert in to MCUXpresso IDE (did that for earlier versions, have not checked if this is still possible with 11.5). see https://mcuoneclipse.com/2017/04/09/mcuxpresso-ide-installing-processor-expert-into-eclipse-neon/ how this would look like. Otherwise: I used KDS to generate everything and then used MCUXpresso (see b))

b) import/port the KDS project with Processor Expert. https://mcuoneclipse.com/2018/07/27/porting-processor-expert-projects-to-mcuxpresso-ide/

I know this is a bit challenging, but worked for me for several projects with devices which are not supported by the NXP MCUXpresso SDK.

I hope this helps,

Erich

 

2,632 次查看
Bert2
Contributor II

Thank you Erich,

that will probably be my way. I did not look into the older IDE because the website did redirect me to the newer one...

Thanks very much!

0 项奖励
回复