How to generate "lin_cfg.c" files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to generate "lin_cfg.c" files

1,105 Views
shenjiaqi
Contributor I

Hello,

   I've a new project by using SKEAZN32.And I want to created LDF and NPF file then generateing  "lin_cfg.c" files by tool,I try to use S32Ds and KDS to do this job,but it doesn't work.So i want to know if  are there some ways to  generate "lin_cfg.c" files by tools.If so, what should I do.

Thanks.

0 Kudos
Reply
1 Reply

972 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi jiaqi Shen,

 

I recommend you to check the following application note in chapter 4.1:

 

Using NXP’s LIN Driver with the MagniV Family

 

For this you will need to download the NXP LIN Driver Package from the following link:

 

LIN2.x and SAE J2602 Stack

 

Please keep in mind that this driver is using CodeWarrior and you will need to install the plug-in in order to create LDF and NPF files (check chapter 3.1 of Eclipse_User_Manual inside the NXP LIN Driver installation folder).

 

I hope this helps you.


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply