How to erase a sector located in FlexNVM of TWRK40 kit? Hardware bug?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to erase a sector located in FlexNVM of TWRK40 kit? Hardware bug?

ソリューションへジャンプ
2,074件の閲覧回数
bugs
Contributor III

TWRK40Kit has a K40X256, I couldn't erase a sector in FlexNVM.

According K20P144M100SF2RM.pdf, page 661

The Erase Flash Sector command is 0x09, it has a 24bit address parameter, but the FlexNVM is located at address 0x10000000, it is above 24-bit address space. How can I erase this FlexNVM?

0 件の賞賛
返信
1 解決策
1,558件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Bit 23 controls which Flash block you're writing to.

 

When required by the command, address bit 23 selects between:

• program flash 0 (=0) block
• (for devices with FlexNVM) data flash (=1) block
• (for devices with program flash only) program flash 1 (=1) block

 

See section 28.4.12 of the K60 RM for more details, but that should get you going! 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,558件の閲覧回数
bugs
Contributor III

All the read/write FTFL commands are 24-bit address? How can we read/write FlexNVM?

0 件の賞賛
返信
1,559件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Bit 23 controls which Flash block you're writing to.

 

When required by the command, address bit 23 selects between:

• program flash 0 (=0) block
• (for devices with FlexNVM) data flash (=1) block
• (for devices with program flash only) program flash 1 (=1) block

 

See section 28.4.12 of the K60 RM for more details, but that should get you going! 

0 件の賞賛
返信