How to ensure headers on a "shield" I am designing will line up with holes on the FRDM KL25Z board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to ensure headers on a "shield" I am designing will line up with holes on the FRDM KL25Z board?

1,191 次查看
MelonM
Contributor II

I am working on a project using an FRDM-KL25Z dev board. I realized that the circuit I am designing is small enough to work well as shield for the board. I have never designed a shield before so I thought it would be a good thing to learn how to do.

I need to ensure that the headers on the shield line up with the headers on the dev board so that the shield can be plugged into the dev board. I have not been able to find any CAD model of the board that would allow me to do this easily. Is measurement with calipers my only option to find these dimensions? I do not own calipers so this would be a problem.

标记 (3)
0 项奖励
回复
3 回复数

136 次查看
carloslop
Contributor I

I also need the mechanical dimensions, but including the board outline since the FRDM-KL25Z will be placed on top of a carrier board. However, I cannot find the design files for the new revision (?) with USB Type C connectors. Are these available?

 

Thanks,

Carlos

标记 (2)
0 项奖励
回复

1,158 次查看
MelonM
Contributor II

I think that the three dimensions indicated in the attached image are all I would need in order to put the pin headers in the right places in kicad. These dimensions must exist somewhere, but I have not been able to find them.

FRDM-KL25Z_BD.jpg

0 项奖励
回复

1,143 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @MelonM ,

Thanks for your post. The FRDM-KL25Z board is designed with pinouts following the Arduino UNO R3 shield standard. You can find the Arduino reference design online to obtain the relevant data.

Alternatively, you can also download the FRDM KL25Z Design Files(FRDM-KL25Z|Freedom Development Platform|Kinetis® MCU | NXP Semiconductors), and open the following files to obtain the data.

Celeste_Liu_0-1737347103893.png

Celeste_Liu_1-1737347184516.png

 

Hope it can help you.

BRs,

Celeste

 

---------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------------------------

 

0 项奖励
回复