How to configure differential ADC on K22FN1M0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure differential ADC on K22FN1M0

Jump to solution
2,700 Views
ARQuattr
Contributor IV

I am using the MQX4.1 lwadc based on the example code for the twrk21f120m board, and for single-ended readings it appears to work fine.  But I also have a differential input on a custom board I want to use and I'm not sure how to set that up.

The source I'm using is ADC0_SOURCE_ADPM1 (pins 14 an 15 on the 100pin K22).  This source (according to adc_mk21f.h) includes the ADC_SOURCE_DIFF flag, so I was hoping it would work without extra effort, but it looks like I'm getting only a single-ended reading.

If I call _lwadc_get_attribute(lwadc_ptr,LWADC_DIFFERENTIAL,&value), I get a response of 0.  If I try to set it (calling _lwadc_set_attribute(lwadc_ptr, LWADC_DIFFERENTIAL, 1)), I get an error.

Are there some other flags or configuration I need to do to get differential readings?

Thanks,

Angelo

Labels (1)
0 Kudos
Reply
1 Solution
2,198 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello Angelo,

Have a look at the SDK, it has drivers for the ADC and it supports differential mode.

For the moment K64,23 and 24 are the only supported, but in the next revision K21 and K22  120 MHz will be supported. But the registers for the ADC are the same, so you will probably be able to reuse most of it.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_SDK

Regards,

Santiago

View solution in original post

0 Kudos
Reply
5 Replies
2,198 Views
ARQuattr
Contributor IV

Gee, nice!

Well thanks for saving me more time on this.  I'll try Processor Expert, or maybe just write my own simple driver.  Or maybe I'll just read each one single-ended and take the difference, although I was hoping for a simultaneous read.

Has anyone else written some simple direct register access code to configure and read differential ADC?

Thanks

0 Kudos
Reply
2,199 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello Angelo,

Have a look at the SDK, it has drivers for the ADC and it supports differential mode.

For the moment K64,23 and 24 are the only supported, but in the next revision K21 and K22  120 MHz will be supported. But the registers for the ADC are the same, so you will probably be able to reuse most of it.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS_SDK

Regards,

Santiago

0 Kudos
Reply
2,198 Views
santiago_gonzal
NXP Employee
NXP Employee

Angelo,

Just as an update, the SDK 1.0.0 has been released in the web. It has examples for K22 120 MHz.

Regards,

Santiago

0 Kudos
Reply
2,198 Views
richardtseng
Contributor I

We ran into the same problem trying to use lwadc to read differential ADC on K60.

Does FSL have plan to add K60 support to SDK ?

Have anyone try adding differential ADC to lwadc ?

Thanks,

Richard

0 Kudos
Reply
2,198 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello Angelo,

If you dig into the code you will see differential pair is not supported in MQX:

\Freescale_MQX_4_1\mqx\source\io\lwadc

File lwadc_kadc.c, line 491:

        case LWADC_DIFFERENTIAL:

            /* We don't support differential, so return FALSE if asked for it, TRUE otherwise */

            return !value;

Have you tried with Processor Expert? I believe it supports differential pair ADC.

Regards,


Santiago