How to configure PWM offset on MKE14F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure PWM offset on MKE14F

ソリューションへジャンプ
2,674件の閲覧回数
kwf
Contributor III

Hi Community

Do the MKE14F FTM_PWM can achieve PWM offset function?

The PWM2 offset Ts/2 than PWM1.

kwf_0-1639375626341.png

 

 

 

0 件の賞賛
返信
1 解決策
2,660件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello @kwf ,

The PWM of the MKE14 can achieve this offset configuration there is no limitation mentioned for this product in the documentation. But this type of configuration does not have an specific function either an SDK example. Please let me know if you have any other question or if I can help you on anything else.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,661件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello @kwf ,

The PWM of the MKE14 can achieve this offset configuration there is no limitation mentioned for this product in the documentation. But this type of configuration does not have an specific function either an SDK example. Please let me know if you have any other question or if I can help you on anything else.

0 件の賞賛
返信
2,654件の閲覧回数
kwf
Contributor III

Hi nxf77486

Is it combine mode? How to configure those register?

Which section in documentation mention PWM offset?

In "Kinetis KE1xF Sub-Family Reference Manual, Rev. 4, 06/2019" 41.5.9 Combine mode 

The channel out put will reset to initial status (High or low depend on ELSB and ELSA register) when count to MOD value. No matter what, the out put is not offset. Did I misunderstand?

0 件の賞賛
返信
2,639件の閲覧回数
kwf
Contributor III

Hi 

I found solution.

Thanks for help!

0 件の賞賛
返信