How to allocate KW38 freedom bootloaderand BLE application storage area?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to allocate KW38 freedom bootloaderand BLE application storage area?

ソリューションへジャンプ
2,160件の閲覧回数
wenhuafeng
Contributor II

Hi everyone,

I use MCUXpresso IDE (V11.2.1) to develop the function of KW38, and use feedom bootloader to boot the BLE application through the UART upgrade of KinetisFlashTool.exe tool, but I don’t know how to allocate the FALSH and RAM space of the BLE application to correspond to the FLASH of the feedom bootloader , RAM space can be upgraded by this method?

 

Freedom bootloader FLASH and RAM space are as follows:

1.jpg

BLE wireless_uart_bm FLASH and RAM space are as follows:

2.jpg

The names of FLASH and RAM, FEFT_2K.cfx, FEFT_2K_D.cfx, do not know what they mean, is there any relevant documentation?

"MCU Bootloader Demo Application User's Guide.pdf", I tried the examples inside, and it can be programmed normally as described in the document.

thank you very much!

0 件の賞賛
返信
1 解決策
2,111件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

You do not modify the application's size. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,134件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

If your bootloader will go to address 0xa000, you can configure like this.

You should modify the application's Location and the size.

4.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,114件の閲覧回数
wenhuafeng
Contributor II

Hi,TIC

Modify here, there is an error message!

1.JPG

0 件の賞賛
返信
2,112件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

You do not modify the application's size. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信