How to activate K60´s 2nd Channel of Flex Timer FTM2 for PWM unter Keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to activate K60´s 2nd Channel of Flex Timer FTM2 for PWM unter Keil

Jump to solution
2,100 Views
tfrauenrath
Contributor III

Hello,

a was able to configure a PWM on the first channel of the FTM2 port on a K60. How can I activate also

the 2nd channel on Pin B19 without influencing with Pin B18?

This is my working code for channel one. Unfortunately there is no "FTM_C0SC_MSB_MASK" or

"FTM_C1SC_MSB_MASK" as example. In "MK60N512MD100.h" there is only "FTM_CnSC_MSB_MASK".

Thank you!

This is the .h file provided by keil:

http://www.keil.com/dd/docs/arm/freescale/k60/mk60n512md100.h

This is my working code for channel 0:

/*-----------------------------------------------------------------------------

* DA_init: Initilizes digital to analog PWM engine

*

* Parameters: (value, channel)

* Return: (none)

*----------------------------------------------------------------------------*/

void DA_init (void) {

/*Enable the Clock to the FTM0 Module*/

SIM->SCGC3 |= SIM_SCGC3_FTM2_MASK;

/*Pin control Register (MUX allowing user to route the desired signal to the pin. */

PORTB->PCR[18] = PORT_PCR_MUX(0x3);

PORTB->PCR[19] = PORT_PCR_MUX(0x3);

/*When write protection is enabled (WPDIS = 0), write protected bits cannot be written. When

write

protection is disabled (WPDIS = 1), write protected bits can be written. The WPDIS bit is the

negation of

the WPEN bit. WPDIS is cleared when 1 is written to WPEN. WPDIS is set when WPEN bit is read as

a 1

and then 1 is written to WPDIS. Writing 0 to WPDIS has no effect.*/

FTM2->MODE |= FTM_MODE_WPDIS_MASK;

/*FTM Disable; Only the TPM-compatible registers (first set of registers) can be used without

any restriction. Do not

use the FTM-specific registers.*/

FTM2->MODE &=~FTM_MODE_FTMEN_MASK;

/*Quadrature Decoder mode is disabled.*/

FTM2->QDCTRL &=~FTM_QDCTRL_QUADEN_MASK;

FTM2->CNT = 0; /*16bit - FTM Counter Value - reset counter to zero*/

FTM2->MOD = 65534; /*Overflow rate; The Modulo register contains the modulo value for the

FTM counter.*/

FTM2->CNTIN = 0; /*Set the Counter Initial Value to 0*/

// // FTMx_CnSC - contains the channel-interrupt status flag control bits

FTM2->CONTROLS->CnSC |= FTM_CnSC_ELSB_MASK; FTM2->CONTROLS->CnSC &=

~FTM_CnSC_ELSA_MASK; /*Capture on Falling Edge Only*/

FTM2->CONTROLS->CnSC |= FTM_CnSC_MSB_MASK; //Channel Mode select

//Status and Control bits

FTM2->SC = FTM_SC_CLKS(0x01); // Selects Clock source to be "system clock" or (01)

//sets pre-scale value

FTM2->SC |= FTM_SC_PS(0x08);

/*activate output*/

FTM2->CONTROLS->CnV = 400;

}


Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,330 Views
paulmartin
Contributor III

Your code only has one mistake with the CONTROLS registers

You need to specify an array index CONTROLS[i].

In your code the value i = 0. That is why you will always change your channel 0 settings when trying to configure channel 1.

This is how I configure 3 PWMs:

FTM0->CONTROLS[0].CnSC = 0x00000028; /* channel configured for edge aligned PWM */

FTM0->CONTROLS[1].CnSC = 0x00000028; /* channel configured for edge aligned PWM */

FTM0->CONTROLS[2].CnSC = 0x00000028; /* channel configured for edge aligned PWM */

FTM0->CONTROLS[0].CnV = 6249; /* start PWM with 100 % duty cycle */

FTM0->CONTROLS[1].CnV = 6249; /* start PWM with 100 % duty cycle */

FTM0->CONTROLS[2].CnV = 6249; /* start PWM with 100 % duty cycle */

You can use the named masks instead of explicit values in CnSC.

View solution in original post

0 Kudos
Reply
1 Reply
1,331 Views
paulmartin
Contributor III

Your code only has one mistake with the CONTROLS registers

You need to specify an array index CONTROLS[i].

In your code the value i = 0. That is why you will always change your channel 0 settings when trying to configure channel 1.

This is how I configure 3 PWMs:

FTM0->CONTROLS[0].CnSC = 0x00000028; /* channel configured for edge aligned PWM */

FTM0->CONTROLS[1].CnSC = 0x00000028; /* channel configured for edge aligned PWM */

FTM0->CONTROLS[2].CnSC = 0x00000028; /* channel configured for edge aligned PWM */

FTM0->CONTROLS[0].CnV = 6249; /* start PWM with 100 % duty cycle */

FTM0->CONTROLS[1].CnV = 6249; /* start PWM with 100 % duty cycle */

FTM0->CONTROLS[2].CnV = 6249; /* start PWM with 100 % duty cycle */

You can use the named masks instead of explicit values in CnSC.

0 Kudos
Reply