How to access PTA2 and PTA3 pins for I2C communication on FRDM-KE02Z board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to access PTA2 and PTA3 pins for I2C communication on FRDM-KE02Z board?

1,534 次查看
mstagg
Contributor I

The board uses PTA2 and PTA3 for I2C communications, but both of these pins are already used by the on-board accelerometer. PTB6 and PTB7 are the other options, but they are running an on-board clock. How can I use I2C communication on this board if all the allocated pins are already used by on-board components?

Please don't yell at me. I'm an intern.

标记 (3)
2 回复数

1,310 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Matthew Stagg,

      

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,310 次查看
mjbcswitzerland
Specialist V

Hi Matthew

I2C is a bus that can have many devices on it so the fact that the accelerometer is connected to PA2 and PA3 don't restrict you from using the same bus lines for furter devices with difference addresses.

Regards

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support  / µTasker FRDM-KE02Z40M support  / µTasker FRDM-KE06Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market