How to Make DMA-UART work with KL05 and series?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Make DMA-UART work with KL05 and series?

1,934 Views
Amit_Kumar1
Senior Contributor II

Hi

I am using code warrior 10.5 along with PE , I wanted to test a program in which I will be sending some commands using terminal window to UART0 and it will be received through DMA and will send it back to the terminal(with or without DMA). I have done this for K20 and other K series and it is working fine. But it didn't work with Kl05 and FRDM-Kl46Z here is the attached code . I tried the sample code present in the codewarrior for MKL05Z32VLF4. and also tried the code given in KLQRG, chapter no 7. even that didn't work. Please look into the matter and resolve this issue.

 

Kind Regards

Amit Kumar

Original Attachment has been moved to: kl05-DMA-testing-23-05-2014.zip

0 Kudos
Reply
1 Reply

1,460 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Amit,

I'd like to suggest that you can refer to low_power_dma_uart_demo in KL25 sample code.

The demo is about UART work with DMA.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply