How do you run a usb example on the the MK22F12810 chip?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do you run a usb example on the the MK22F12810 chip?

5,424 Views
brendanmerna
Contributor IV

I have the smaller slower version of the MK22F chip set on my custom board the MK22F12810 chip. I'd like to get a USB stack running on this chip, but there isn't a usb platform build for this chip. I've successfully used the FRDM-K22F board and ran a simple keyboard hid usb application. Is there a way I can modify the MK22F51212 platform, so I can build and run the same keyboard demo on the MK22F12810 chip? Or is there another approach I should be doing to get this kind of application running?

Tags (2)
24 Replies

4,540 Views
brendanmerna
Contributor IV

Mark,

Thanks for your help. With your guides I was able to upgrade the code 2.0 now and have gotten a working USB composite device example. 2.0 seems to be better just because everything is contained in one area.

-Brendan

0 Kudos
Reply

4,539 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer could visit here to create MCU SDK software package for MK22FN128xxx10 product:

pastedImage_3.png

The USB demo project located at below default path:

..\SDK_2.2_MK22FN128xxx10\boards\frdmk22f\usb_examples

Thank you for the attention.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,540 Views
brendanmerna
Contributor IV

Ma Hui,

I was able to build this and found the USB project. But, don't I still need a library to build with this project?

-Brendan

0 Kudos
Reply

4,540 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Brendan,

The USB stack was embedded in MCUXpresso SDK software package. Thanks.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,540 Views
brendanmerna
Contributor IV

Hey Ma Hui,

So, unlike using the KSDK 1.3 package I don't have to build any of the platform libraries if I use the MCUXpresso tool. I just build whatever project I'm using?

-Brendan

0 Kudos
Reply

4,540 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Brendan,

The MCUXpresso SDK software is different with original KSDK V1.3, customer can use config setting to build a SDK package for one product(or hardware evaluation board).

Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,540 Views
mjbcswitzerland
Specialist V

Hi

Take a look at
http://www.utasker.com/kinetis.html
- http://www.utasker.com/kinetis/FRDM-K22F.html
- http://www.utasker.com/kinetis/TWR-K22F120M.html
- http://www.utasker.com/kinetis/BLAZE_K22.html
- composite devices http://www.utasker.com/kinetis/USB_Device.html
- User's guide http://www.utasker.com/docs/uTasker/USB_User_Guide.PDF

which includes USB stack which is compatible with all K22 parts (just needs SIZE_OF_FLASH and SIZE_OF_RAM set accordingly and adapts itself to the part in question).
Also the USB operation can be simulated in Visual Studio (including interrupt and DMA operation) for learning and operation reviews in critical applications.

Regards

Mark

0 Kudos
Reply

4,540 Views
brendanmerna
Contributor IV

Hey Mark,

I haven't used utasker yet. Can I get a little more information on how this would work? I have the KSDK 1.3 and my assumption would be that I just need to figure out how to build a USB library that's compatible with this chip. 

-Brendan

0 Kudos
Reply

4,540 Views
mjbcswitzerland
Specialist V

Hi

In the uTasker project you just enable the define USB_INTERFACE and the class (or classes) that you want (eg. USE_USB_CDC and how many interfaces, USE_USB_MSD, USE_USB_HID_MOUSE, USE_USB_AUDIO etc.) and you have a complete operating project for any Kinetis part with USB (KL, KV, K etc.). It is fully integrated and you can even add USB-RNDIS TCP/IP operation by simply enabling USB_CDC_RNDIS.

It is designed for professionals who require immediate and proven operation for fast reliable product completion, complete product operation simulation without porting worries or IDE dependencies. It doesn't require libraries to be built and its integrated USB class and drivers are compatible with all Kinetis parts.

Regards

Mark

0 Kudos
Reply

4,540 Views
brendanmerna
Contributor IV

Mark,


uTasker doesn't have a project for the chip I'm talking about MK22F12810. Is there a compatible project that I should select?

-Brendan

0 Kudos
Reply

4,540 Views
mjbcswitzerland
Specialist V

Brendan

NXP specifies using the FRDM-K22F
http://www.utasker.com/kinetis/FRDM-K22F.html
or the TWR-K22F120M
http://www.utasker.com/kinetis/TWR-K22F120M.html
for developments aimed at K22F128 100MHz parts.

Therefore it is best to select the FRDM_K22F target and then adjust its configuration to suit the final chip.
The open source uTasker version doesn't have full K22F128 100M support but it is very easy to adapt.

#define FRDM_K22F

1. Specify the speed to be 100MHz max.
    #define KINETIS_MAX_SPEED    100000000
2. Since the chip has much less SRAM reduce the heap size, eg
    #define OUR_HEAP_SIZE        (HEAP_REQUIREMENTS)((12 * 1024) * MEM_FACTOR)
3. In app_hw_kinets. adjust the Flash and RAM sizes:
    #define SIZE_OF_FLASH       (128 * 1024)                             // 128k FLASH
    #define SIZE_OF_RAM         (24 * 1024)                              // 24k SRAM
4. It will be necessary to edit kinteits.h so that the SRAM addressing is correct by adding (at the appropriate location)
#elif defined KINETIS_K22 && defined KINETIS_K_FPU && (SIZE_OF_RAM == (24 * 1024))
    #define RAM_START_ADDRESS   (0x20000000 - (8 * 1024))                // SRAM L is 8k and is anchored to end at 0x1ffffffff
                                                                         // SRAM H is the remainder of RAM size and is anchored to start at 0x20000000

5. You will need to use also a linker script file that matches.
For example use K_128_16.ld and modify two lines
SRAM (wx)  : ORIGIN = 0x1fffe1f0, LENGTH = 0x00006000-0x1f0
__SRAM_segment_end__     = 0x20003fff;
to increase form 16k to 24k SRAM

The USB is compatible.

These are the (main) differences between the K22F512 120MHz and K22F128 100MHz

K22F128 has 2 SPIs, no USB-CD, no FTM3, no CMT, but has an I2S. There are only 4 DMA channels available.
All (available) interrupts are compatible so as long as non-existent channels are not attempted to be used all should be fine.

If you want to tune a little more exactly (shouldn't be really necessary) you can add/adjust these in kinetis.h

#elif defined KINETIS_K22
    #if ((SIZE_OF_FLASH == (512 * 1024)) || (SIZE_OF_FLASH == (256 * 1024)) || (SIZE_OF_FLASH == (128 * 1024)))
        #define UARTS_AVAILABLE     3
    #else
        #define UARTS_AVAILABLE     6
    #endif

#elif defined KINETIS_K22
    #if ((SIZE_OF_FLASH == (512 * 1024)) || (SIZE_OF_FLASH == (256 * 1024)) || (SIZE_OF_FLASH == (128 * 1024)))
        #define LPUARTS_AVAILABLE   1
        #define LPUARTS_PARALLEL                                         // LPUARTs and UARTs are counted from 0

    #elif defined KINETIS_K22 && (SIZE_OF_FLASH == (128 * 1024))
        #define DMA_CHANNEL_COUNT    4

#elif defined KINETIS_K22 && (SIZE_OF_FLASH == (128 * 1024))
    #define SPI_AVAILABLE           2

Any project that runs on the FRDM-K22F (K22F512 120M) should be able to run on a K22F128 100M by switching between 1, 2, 3 and 5 settings (1, 2 and 3 are usually controlled by a single define once a real target is set up).

Regards

Mark

4,540 Views
brendanmerna
Contributor IV

Mark,

Thank you for the detailed changes. I'll check these out. It might take me awhile as I'm not familiar with the 2.0 SDK or utasker.

Still my biggest problem is I'm using  the KSDK 1.3 package right now and have a lot of code developed for it. I'd like to keep using this SDK because I'm comfortable with it and would like to acoid porting it over to the 2.* SDK. You mean more familiare with utasker, but is there away to do these same changes you mentioned, but with the KSDK 1.3. For example modifying the usbd_sdk_bm_lib_MK22F51212 to be compatible and build with the ksdk_platform_lib_K22F12810?

When I tried to build there was errors on defines missing, so if the USB is compatible between the 2 chips then I just need the right defines to add/take away stuff.

-Brendan

0 Kudos
Reply

4,540 Views
mjbcswitzerland
Specialist V

Hi Brendan

In fact it should be very easy to move from the K22F120 to K22F100 parts in any environment with framework that anticipates this. I tried once with a KSDK version and with good processor knowledge it is possible but does require quite a lot of work. You need to make a new directory structure for the new part and rename lots of files so they fit in (and don't conflict) - there is a thread where I did this about 18 months ago as exercise at the SDK forum - then modify the things that are different. The differences can be just a few lines of code in some cases but it did need about 500MBytes of new files to be added to be able to actually do it without disrupting everything else. When the next SDK version comes along all work is of course lost again...maintenance is also difficult because lots of different projects need to be modified and maintained for each single change.

If you send me your project (I can give you a free protected GIT account in case you need to keep it secure) I can take a quick look. We offer a free porting service which will allow you to then simulate the project - the uTasker environment is many times more efficient than the one that you have been using and porting a project to be smaller, faster and more modular can usually be achieved in a very short time. Afterwards you will find you can develop much more efficiently and usually greatly shorten project development times.

Depending on the complexity you already have I may be able to send you a complete operating project for your new part so you don't need to go through the usual days and week of tweaking the various incompatible libraries.

Regards

Mark

If you want to give it a quick try, send a contact mail to an address at http://www.utasker.com/support.html - don't get frightened because it is FREE and you may find it will save your company many thousands of $ in the long run.

4,540 Views
brendanmerna
Contributor IV

Mark,

I have a .zip file for the project working with the KSDK 1.3, builds with the ksdk_platform_lib_K22F12810 that I can send to you.
How would you like me to do that?

I also already have the project version controlled, so we don't have to worry about screwing it up too bad.

The project isn't too complex right since I haven't been able to add any api commands, so its just some supporting code for a few sensors and some buttons.

I would assume all the changes would have to be done in the usbd_sdk_bm_lib_MK22F51212. Is that what you did in that post? Can you provide me a link that that?

I also wanted to note at the end that this is for our evaluation board. We weren't able to acquire the 512 chip in enough time to use it with the eval boards, but it will be used in our production units. It's a obnoxious because will have to port the project back and forth because we need to make sure the hardware design (especially USB) is working.

Thanks for the help! I'll let you know on the utasker stuff.
-Brendan

0 Kudos
Reply

4,540 Views
mjbcswitzerland
Specialist V

Brendan

In that case just send the zip file you have (ensure it has no *.exe or *.bat files in it because they may cause it to get blocked) to one of the addresses at the link.

I'll then take a look and advice.

You will find that the uTasker project uses a different concept. It has a single project which will run on about 50 different Kinetis references board and allows moving between Kinetis parts with almost no effort. You can switch between your temporary and final processor with easy and so it solves the deficiencies that you are presently encountering with the NXP libraries.

>>Can you provide me a link that that?
I just searched the other forum but couldn't locate my post from then (sorry) and I did it only as an exercise to help someone trying to use an unsupported part so don't have a backup of it. It is presumably there (or maybe in the KDS forum?) somewhere but I have posted thousands of times in the forums and this makes it difficult to locate specific ones....

Regards

Mark

0 Kudos
Reply

4,540 Views
brendanmerna
Contributor IV

Mark,

Not sure why, but I can not figure out how to attach this .zip file to forum. Can you tell me how to do that or provide an email for me to send it to?

-Brendan

0 Kudos
Reply

4,540 Views
mjbcswitzerland
Specialist V

Brendan

You can use an email address at the link.

To attach to the forum post you need to first click on "Use advanced editor" (top right of the thread reply).
then you will have "Attach" in the bottom left corner.

Regards

Mark

0 Kudos
Reply

4,538 Views
brendanmerna
Contributor IV

Mark,

Awesome thanks! Here you go.

-Brendan

0 Kudos
Reply

4,538 Views
mjbcswitzerland
Specialist V

Hi

I couldn't get the project to build as you sent it due to some missing items (or incompatible paths). Not being a fully self-contain project makes it difficult to build it in a different environment.

Therefore I just checked through the code and made a FRDM-K22F board project that does the same. You have a lot of unused source files (prepared for later) which are pretty much all using the two I2C buses. Therefore I just enabled the accelerometer I2C interface so that it shows this in operation (it uses the I2C bus at about 100% load to poll the accelerometer as fast as possible).

I enabled USB-CDC and USB-MSD to allow the internal Flash and SRAM to be shown as hard drives. There is a full command line interface on the UART (OpenSDA VCOM) and also on the USB-CDC interface when connected.

Your main() application has been modified to do the same but without needing to poll (interrupt driver state event) and the K22 sleeps whenever it is not needed to be working to save power. The board is simulated to test all of the operation (and simpler debugging).
I couldn't make out exactly what clock your code uses but I set up to run from the internal 48MHz (using USB clock synchronisation "crystal-less"), 24MHz Flash and Bus - I have a feeing that you may have been operating from the 32kHz clock but this isn't suitable for USB. In any case I enable the RTC from 32kHz oscillator and give it a complete Gregorian calendar system.

I then added a K22F128 target which can be switched to with a define K22F128_100M (instead of FRDM_K22F) (also its corresponding linker script needs to be used due to the memory size differences) and this operate the same on the other chip (with USB). This setup also activates the errata for the 0N75K mask (rather than errata for the 0N50M mask).

You could use the I2C code that you have if you don't mind continuing with blocking operation or you could use the uTasker I2C interface instead for non-blocking operation and better performance, but it would require modifications to the general method.

If you pull the uTasker Open Source project you will find that it now has a define called SPECIAL_TEST in the file application.c where I have planted your code as operating in the main loop (modified so that it is fully interrupt driven and doesn't need to poll).
In config.h there is a new define K22F128_100M so switching between this and FRDM_K22F allows moving between the two board/processors.
You will recognise your code and see the simpler method of configuring the interrupt operation - when any key changes your original polling function is called via a system interrupt event (not in the interrupt).

The buttons and outputs can be simulated if you build the project in Visual Studio so you can click on the inputs to test their interrupt and see the outputs changing in response to your code handling the changes.

It took about 1.5 hours to port your project to the environment on both FRDM-K22F and K22F128-100M targets, add USB and various other features and test on the K22F512-120M. I don't have a K22F128 target but I have tested the operation in the simulator and expect it to run the same on HW (if not it will be a minor detail which can be easily fixed).

If there is anything you don't understand just ask - I certainly recommend building in Visual Studio (in fact it is also possible to debug on the target directly for Visual Studio if Visual GDB is used) so that you can simulate, test and debug the project since it is so much faster than working on the target. If you have difficulties and I find a few minutes I'll maybe post you a video showing your project operating, illustrating the keys' interrupt operation.

Regards

Mark

4,538 Views
brendanmerna
Contributor IV

Mark,

First of all thank you for all your hardwork, I greatly appreciate it!

How do I find this modified project on utasker you are talking about?

-Brendan

0 Kudos
Reply