How do i find out the explanation or the definition to the abbreviations for the i/o pins on the kl02 32 pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do i find out the explanation or the definition to the abbreviations for the i/o pins on the kl02 32 pin?

1,535 次查看
blazerogers
Contributor I

How do i find out the explanation or the definition to the abbreviations for the i/o pins on the kl02 32 pin mcu? For example some of the ones that are listed are PTB, PTA,IRQ, VREFH, and VREFL. Anything will help, thanks.

0 项奖励
回复
1 回复

1,418 次查看
mjbcswitzerland
Specialist V

Hi Blaze

I don^t think that there is a general abbreviation list but if you search for tehe one that you are interested in in the user's manual there will be a description of it.

Basically all with PTx are GPIOs. PTA1 is Port A bit 1, for example and PTC5 is Port C bit 5, and so on

VREFH and VREFL are the ADC's voltage reference pins (high [highest level reference] and low [lowest level reference])

IRQ is the interrupt function that some pins can be programmed to have.

KBI0_Px is the keyboard interface function that a pin can be programmed to have.

FTMx for FlexTimers

Etc.

There is then a chapter detailing each module.

Regards

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support / µTasker FRDM-KE02Z40M support / µTasker FRDM-KE06Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复