How do I selsct a MCU with just an .axf file to write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I selsct a MCU with just an .axf file to write

1,005 次查看
erik_hedberg
Contributor I

how do I select an MCU with just an .axf file to write

0 项奖励
回复
1 回复

979 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Erik,

Hope you are doing well.

Could you please share what microcontroller you are using so I can provide detail instructions if needed. 

If you are working with MCUXpresso IDE, you may download the SDK of the microcontroller you are using on the MCUXpresso Website

Once downloaded, you may import the SDK to MCUXpresso IDE, then you can import an example. 

When you build the project, the axf file is created automatically.

pastedImage_2.png

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复